Opening SAP View From FlashPro
There are two ways to access the SAP View.
- From the Flash Order
- From the Order Search Screen
From the Flash Order
Step 1: Open the order for which you want to see the SAP Status. Remember, the order should be in the 'Submitted-Accepted' status.
Step 2: Go to the 'View' menu and select 'SAP View'.

This opens the SAP View page.

From the Flash Order Search Screen
Note: Be sure to have the Flash Order Number OR the SAP Order Number at hand. You would need either one of the two to open the SAP View from the order search screen, but you do not need both.
Step 1: Open the Order Search Screen and enter the Flash Order Number OR the SAP Order Number

Step 2: Select the 'SAP View' checkbox, and click on 'Search'. This opens the SAP View page.